AXIS#.IL.PWMFREQ
Description
This parameter provides the current loop PWM frequency for the specified axis.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
kHz |
|
Range |
0 to 781.250 kHz |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.IL.PWMFREQ |
500ah |
2eh |
Unsigned32 |
- |
1000:1 |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5823 |
1 |
5823 (0x16bf) |
AXIS1.IL.PWMFREQ |
Unsigned32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.IL.PWMFREQ |
5823 |
Float |
Read Only |
- |